工程师你好,
我们选用TPS564201,将12V降低至5V,原理图如下所示,电感选型为3.3uH,温升电流为3.3A。
5V后级负载为10个隔离电源模块(5V转隔离5V),其中有7个模块,各接1个隔离RS485芯片,另外1个模块,接一个5V转12V的BOOST电路,另外2个模块,各接一个转5V负压的电荷泵芯片。
目前上电后,主电路的电感有啸叫情况,请问是否为电感感量选型过小导致的?需要选4.7uH的么?
感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.