This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: 关于CE管脚上电后芯片明确的启动时间

Part Number: BQ24610


Hi  TI工程师您好,我们在使用BQ24610芯片时需要做电池检测,情况就是当CE管脚上电时,BQ24610芯片开始工作,充电使能引脚(CE)和充电器的软启动过程。根据数据手册,CE引脚上电后,充电器的软启动过程通常需要大约1.5秒,从CE引脚上电到充电器开始正常工作,整个过程大约需要1.5秒加上软启动的时间(8个步骤,每个步骤1.6毫秒),总共大约需要1.5秒加上12.8毫秒(8个步骤 × 1.6毫秒/步),再到STAT1和STAT2管脚电平发生变化时间我们使用示波器抓出时间为1.63s(大概),希望TI工程师给我们一个确定的时间,从CE管脚使能之后到STAT管脚发生变化的时间,谢谢