This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531带载能力问题

Other Parts Discussed in Thread: TPS54531

我的设计是用TPS54531实现24V转18V,3A输出。

画原理图和PCB图之前用Webench仿真了一下,调压电阻选的是10k欧和470欧(计算得17.82V)。

带载试了一下,100欧负载输出为18.2V;30欧负载输出为19.4V,听见有嗞嗞的响声;8欧负载输出为5.5V而且不稳定,有嗞嗞响声。

我怀疑我选的元器件是否有问题,电容选的是国产4326的钽电容,输出端是2个35V-10uF的钽电容(Webench里是4个4.7uF),然后为了降低阻抗,输出端钽电容并了一个0.1uF的陶瓷电容。

电感我用的是国产功率电感SMRH127-10uH,额定电流4A,但是阻抗没有满足Webench的要求。另:Webench里标的阻抗是直流阻抗还是测试条件为多少kHz下的阻抗?

1. 请问,带载能力差跟电容和电感的阻抗关系大吗?

2. 设计原理图和PCB的时候,我犯了个错误,输出端未接地。我现在是把输出端钽电容的负端飞线接地,这个对带载输出影响大吗?

3. 带载听到嗞嗞的响声是正常现象吗?