专家好!
我设计了一个仪表产品,选用了TLV70033将3.6V的电池输出稳压在3.3V。一批产品中(200个为一批),总有3~5个LDO器件在使用一段时间后发生损坏,搞不清什么原因。请专家指教!谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家好!
我设计了一个仪表产品,选用了TLV70033将3.6V的电池输出稳压在3.3V。一批产品中(200个为一批),总有3~5个LDO器件在使用一段时间后发生损坏,搞不清什么原因。请专家指教!谢谢
你好,这应该不会发生的,这失效率太高了,是什么情况造成了芯片的损坏,过热?应该不会。是不是有静电,谢谢。
收到回复,非常感谢!
我们的确遇到这样问题。我们仪表的工作电流是50mA左右,应该不存在过热现象。芯片出现问题是输入3.6V时,损坏芯片输出在1.8V、2.4V、2.8V情况都有(低于3.0V时我的仪表就不能正常工作了)。电路设计中,输入输出电容的布板按说明书要求做了,电容靠近管脚。我们输出电容使用的是1uF,但输入电容使用的是0.1uF陶瓷电容与10uF电解电容并联,输入电容有问题吗?我们第一批提交的100套仪表没出现任何问题(LDO器件独立购买、且请第三方单位进行老化筛选),但第二批200套已出现5个LDO有问题了(器件也是在同一供货商,也请第三方单位进行老化筛选)。如果电路电容没问题,可能就是静电了(这个季节本地干燥,操作人员有时不带防静电手环)。三防漆处理过厚(如覆盖LDO全部)会有问题吗?谢谢您的帮助!