LM5123-Q1: LM5123与LM5122

Part Number: LM5123-Q1
Other Parts Discussed in Thread: LM5122

您好,我用webench查看了输入12V~18V, 输出55V 6A的方案,并看了很多以往的帖子,因为空间比较小,不能确定用多项还是单项,单项感觉电路简单些,时间紧,请教两个问题,非常感谢!

1. 推荐芯片方案中的LM5123Q,当设置输出电流大一点时,比如输出从4A调整到4.5A时,推荐的方案中mosfet的电压要求就从100V提高到155V,想问一下,要求Vds 155V的mosfet,我可以用100V的代替吗?该方案用于工业升压应用,可靠性要求还是比较高的

2.同样的参数感觉LM5123Q比LM5122对mosfet的要求低,故是不是LM5123Q技术更新,更合适大功率输出一些呢?我要选LM5123Q还是LM5122呢?如果要降低mosfet的电压要求,有其它办法吗?

2.用LM5123的话,电容数量多,电感值小和mos电压高等,能帮我审一下这个方案可行不?

3.另外有支持2项的单芯片方案没?可能综合空间比单项的小,问题有点多,再次感谢老师!