我用LM51551升压的150V,22uH电感额定电路5A左右,MOS的通流18A;
现象1:无输出负载,当输入是6.3V时,后端输出只有80V左右,无电感发热问题;
现象2:无输出负载,当输入是12V时,后端输出150V,但10s以后出现电感和MOS严重发热现象,非常烫,导致MOS器件损伤;
现象3:无输出负载,当输入是20V时,后端输出150V左右,无电感MOS发热问题;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
输出150V电压,采用反激式(带变压器的拓扑)或升压 + 电荷泵(无变压器),建议采用数据手册“Figure 10-8. LIDAR Bias Supply 2”的电路拓扑。
选择这两种拓扑之一的原因是器件的占空比限制。
占空比计算为 1 - Vin/Vout,器件需要按规格运行(8.5 Electrical Characteristics)。
LM5155x 2.2-MHz Wide Input Nonsynchronous Boost, SEPIC, Flyback Controller datasheet (Rev. E)
在链接中的芯片产品网页上提供了“计算工具””辅助电路设计。