This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51551: 设计升压150V,不同输入电压对应的表现不同,甚至出现MOS损坏的原因分析

Part Number: LM51551


我用LM51551升压的150V22uH电感额定电路5A左右,MOS的通流18A

现象1:无输出负载,当输入是6.3V时,后端输出只有80V左右,无电感发热问题;

现象2:无输出负载,当输入是12V时,后端输出150V,但10s以后出现电感和MOS严重发热现象,非常烫,导致MOS器件损伤;

现象3:无输出负载,当输入是20V时,后端输出150V左右,无电感MOS发热问题;