This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: FCC 衰减和电池激活

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: EV2400,

Hi

关于客户电池激活和FCC 衰减问题,还请帮忙确认下。谢谢

1. 我们带PRES使用功能的电池遇到一个问题:电池15天搁置后,进入到ship模式,然后短接电池上的PRES脚到P-,电池使用直流电源8.7V/2A进行充电,电池无法唤醒激活。但是当我们使用EV2400通信盒连接上位机同时对电池进行通信下,可以正常使用直流电源充电激活电池。电池激活后我们使用上位机软件发送shutdown命令,使电池进入到shutdown后,同样短接电池的PRESP-,使用直流电源8.7V/2进行充电可以激活电池,此时电池无需连接通信,单独使用直流电源充电就可以激活。

2. BQ40Z50-R1芯片4串笔记本电池,电池搁置半年到1年时间里,一直处于shutdown模式,半年或一年后进行充电唤醒,FCC更新后是否存在严重衰减的问题。比如说:4500mAh的设计容量,FCC衰减为:2000mAh或者500mAh???