This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54A20: Unable to drive the load

Part Number: TPS54A20


Hello, engineer from TI.

When I am using the TPS54A20 , I am referring to the TPS54A20-EVM770. However, instead of using a 4-layer board, I am using a 2-layer one. But the output voltage I get is always not similar to that of the EVM, and it cannot drive a load. The output voltage keeps fluctuating between 1.19V and 1.21V. The measured waveform at the SW pin is also different from that of the EVM board. The only differences between them are the layout and the package of the components, and all other parameters are the same. But the output is always incorrect. In addition, I also want to ask that it is mentioned in the manual that when the voltage of the series capacitor exceeds 65% of the input, it will enter protection. I wonder if there will be a soft start process during this.