Part Number: LM51770
Other Parts Discussed in Thread: LM25148, LM5148
LM51770芯片的FB电压为1V。为什么该芯片最小输出电压只能到3.3V?
另外 LM5148和LM25148是pin to pin的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您对TI产品的关注!
关于你的咨询,LM51770芯片的FB电压为1V。为什么该芯片最小输出电压只能到3.3V的原因如下。
LM51770采用了已经预设的调节器架构,这种架构决定了其工作范围。
为了保证在负载变化和输入电压波动时的稳定性,设计上往往设定一个最低输出电压,这有助于优化转换效率。
3.3V是现代电子设备中常见的逻辑电平,很多应用都需要这个电压作为基础,因此芯片设计时会优先考虑这一市场需求。
芯片内部的设计和控制电路可能在某些信号电平上需要维持一定的工作参数,因此设定了较高的输出电压限制。
LM5148和LM25148不是pin to pin的,如果是的话芯片主页通常都会有提示。