Other Parts Discussed in Thread: BQ24650
最近在调试BQ24650这款芯片遇到一个问题,输入电压25V,MPPT电压设备为18V,电流设置为1A,输出电压设置为16.3V;调试时MPPSET引脚电压为1.72V,TS引脚电压为2V,Vref引脚电压为3.36V,VFB引脚电压为2.12V,RGEN引脚电压为6V,测量MOS管的开关频率发现不对,很混乱的频率,有570KHZ的开关频率也有190多KHZ的频率,不知道是什么原因造成的。下面两张图是用示波器捕获的