This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: 电池电压是3.3V左右各项功能正常,一旦电池电压是超过3.6V左右就无法正常工作。(已配外部分压电阻和VEN等设置)

Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO

Hi

  TI Team:

   1、设计2节磷酸铁锂串联,最大电压7400mV,电路图如下:

   2、主要的Data memery配置如下:

     Voltage Divider:8500  ;Number of Series Cells:2    Flash Update OK Voltage:0 mV  ,   VEN_EN = 1

    详情见附件 bq34110.gg

  3、   我直流电源模拟电池(真实电池也一样),当电池电压是3.3V时,各项功能正常,电压、电流、温度以及IIC波形均正常。

4、我的问题是:电池电压变更到6600mV(3600以上),bqstudio 与 bq34110 通讯就开始卡顿,读出数据电压、电流、温度等不正确。通讯也不畅,时通时不通。

bq341100.gg.csv

请帮我看看,是哪里配置错了?