Hello,
There are some battery on the market, and want to update the ASCD & AOLD parameters. There is an problem when update the parameters.
1. If flash the FM directly, the Calibrated Parameters will be reset.
2. If change the ASCD & AOLD parameters by hand, there may be some manual error during handling.
So the question is that:
Is there any tool or solution to automatic update the ASCD & AOLD paremeters, and not impack the others?
Looking forward to your reply,
Best wishes!