This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5576: 输出带载后存在无法启动问题

Part Number: LM5576


产品应用:高压电力传输线CT感应取电装置。取电CT为主取能途径,只有在取电CT取能不足时才会使用太阳能取能,CT取能经ACDC转换后(带限压)输入给LM5576然后输出稳定电压给负载供电。

系统框图:

LM5576部分原理图:

问题描述:

由于高压电力线上电流波动,会导致经过取能CT后的交流电压不稳定,假设LM5576输出14.3V带载10W,在取能CT获得的能量足够的情况下,LM5576正常启动,但是当电力线上电流变小到一定程度时,CT取能不足导致LM5576输出无法带动10W负载,这是输出电压低于1V,电流1-2A,实际功率约1W,这种情况下,电力线电流又变大,足够带动10W负载,但是LM5576依然无法输出,还是维持原状。请问这种情况如何解决?

联系方式:980376998@qq.com