This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: 关于的器件几种工作模式

Part Number: BQ25792


您好,我在使用BQ25792时不确定我的设计满不满足使用场景,以下是我的具体使用情况:

1.有外部VBUS输入、无电池,通过SYS为系统供电;

2.有外部VBUS输入、有电池,通过SYS为系统供电同时为电池充电;

3.无外部VBUS输入、有电池,通过SYS为系统供电同时通过VBUS输出为外部供电。

请帮忙评估下BQ25792能否满足我的需求。还有一个疑问,PMID引脚的具体作用是什么,没有用到是否可以悬空?

  • 您好

    1.有外部VBUS输入、无电池,通过SYS为系统供电;

    2.有外部VBUS输入、有电池,通过SYS为系统供电同时为电池充电;

    3.无外部VBUS输入、有电池,通过SYS为系统供电同时通过VBUS输出为外部供电。

    请帮忙评估下BQ25792能否满足我的需求

    根据datasheet的说明应该能满足您的功能要求。

    PMID引脚的具体作用是什么

    Q1 MOSFET Drain Connection – An internal N-channel high side MOSFET (Q1) is connected between PMID and SW1 with drain on PMID and source on SW1. The recommended capacitors at PMID are 3 pieces of 10μF and one piece of 0.1μF ceramic capacitors. Place the 0.1μF ceramic capacitor as close as possible to the charger IC.

    没有用到是否可以悬空?

    datasheet的建议是通过一个电容接地。