This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 充电高温保护后提示有充电电流

Part Number: BQ76952


hi请教一个问题,bq76952充电高温保护后提示有100mA充电电流,充电MOS已经关闭了。实际没有进行充电了。还提示有电流,待温度将至40℃后,电流消失了,可以正常进行充电放电。请问一下,这个是什么原因呢?

  • 您好,

    高温下,周边电路可能受到温度影响,电流检测出现误差。而实际上充电MOS已经关闭,电流并未通过。

    当温度降低至40℃以下时,其周边电路的温度影响减弱。系统不再检测到错误的充电电流。