This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM863252: 芯片内部电感值为多少?

Part Number: TPSM863252

使用TPSM863252做Inverting buck-boost 反压输出电路。输入6.5V 输出 -6.5V@ 0.5A。想知道内部电感值大小,以确定电感的IPeak与IValley 是否会损坏内部开关管。

Using the TPSM863252 to design an inverting buck-boost output circuit. Input voltage is 6.5V, output voltage is -6.5V at 0.5A. I want to know the internal inductor value to determine whether the inductor's peak current (IPeak) and valley current (IValley) could damage the internal switch.

x 出现错误。请重试或与管理员联系。