Part Number: BQ25756
Hi




This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25756
Hi




Hi
麻烦发一下邮箱地址,把完整的设计资料转发到邮箱进行查看。截取了部分设计图纸如下:
设计原理图如下:


PCB布局与layout如下:







上电后整个充电过程运行检测的log如下:
[18:01:05.369]收←◆app start:12
[18:01:08.331]收←◆0x14: 00
0x15: 00
charge vol: 0004
charge cur:012C
Input cur: 0140
Input Vol: 0348
ADC Ctrl-0: 0360
contrl: C9
contrl: C9
[18:01:10.350]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 92
[18:01:11.358]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:12.366]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:13.373]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:14.382]收←◆21: 00
22: 80
23: 00
24: 02
25: 61
26: 80
27: 82
[18:01:15.390]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:16.397]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:17.405]收←◆21: 00
22: 00
23: 00
24: 80
25: 61
26: 80
27: 82
[18:01:18.414]收←◆21: 03
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:19.421]收←◆21: 03
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:20.429]收←◆21: 03
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:21.438]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:22.446]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:23.453]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:24.461]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:25.470]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:26.478]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:27.485]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:28.494]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:29.502]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:30.509]收←◆21: 00
22: 80
23: 00
24: 00
25: 61
26: 80
27: 82
[18:01:31.518]收←◆21: 03
22: 80
23: 80
24: 80
[18:01:31.571]收←◆25: 80
26: 80
27: 80
[18:01:32.651]收←◆21: 81
[18:01:32.677]收←◆22: 81
23: 81
[18:01:32.729]收←◆24: 81
25: 81
[18:01:32.779]收←◆26: 81
[18:01:32.805]收←◆27: 81
[18:01:33.833]收←◆21: 81
22: 81
[18:01:33.884]收←◆23: 81
[18:01:33.910]收←◆24: 81
25: 81
[18:01:33.962]收←◆26: 81
27: 81
[18:01:35.015]收←◆21: 81
[18:01:35.040]收←◆22: 81
23: 81
24: 81
[18:01:35.119]收←◆25: 81
[18:01:35.145]收←◆26: 81
27: 81
[18:01:36.198]收←◆21: 81
[18:01:36.224]收←◆22: 81
23: 81
[18:01:36.276]收←◆24: 81
[18:01:36.302]收←◆25: 81
26: 81
[18:01:36.354]收←◆27: 81
[18:01:37.381]收←◆21: 81
22: 81
[18:01:37.433]收←◆23: 81
[18:01:37.459]收←◆24: 81
25: 81
[18:01:37.511]收←◆26: 81
[18:01:37.537]收←◆27: 81
[18:01:38.564]收←◆21: 81
[18:01:38.590]收←◆22: 81
[18:01:38.616]收←◆23: 81
24: 81
[18:01:38.668]收←◆25: 81
[18:01:38.694]收←◆26: 81
27: 81
[18:01:39.747]收←◆21: 81
[18:01:39.773]收←◆22: 81
23: 81
[18:01:39.825]收←◆24: 81
[18:01:39.850]收←◆25: 81
26: 81
27: 81
[18:01:40.930]收←◆21: 81
22: 81
23: 81
[18:01:41.008]收←◆24: 81
25: 81
26: 81
[18:01:41.085]收←◆27: 81
[18:01:42.113]收←◆21: 81
22: 81
[18:01:42.164]收←◆23: 81
24: 81
25: 81
[18:01:42.243]收←◆26: 81
27: 81
[18:01:43.295]收←◆21: 81
[18:01:43.322]收←◆22: 81
[18:01:43.348]收←◆23: 81
24: 81
[18:01:43.399]收←◆25: 81
26: 81
27: 81
[18:01:44.479]收←◆21: 81
[18:01:44.505]收←◆22: 81
23: 81
[18:01:44.557]收←◆24: 81
[18:01:44.583]收←◆25: 81
26: 81
[18:01:44.635]收←◆27: 81
[18:01:45.662]收←◆21: 81
22: 81
[18:01:45.714]收←◆23: 81
[18:01:45.740]收←◆24: 81
25: 81
[18:01:45.792]收←◆26: 81
[18:01:45.818]收←◆27: 81
[18:01:46.845]收←◆21: 81
22: 81
[18:01:46.897]收←◆23: 81
24: 81
[18:01:46.948]收←◆25: 81
[18:01:46.974]收←◆26: 81
27: 81
[18:01:48.028]收←◆21: 21
[18:01:48.054]收←◆22: 21
23: 21
[18:01:48.106]收←◆24: 21
[18:01:48.132]收←◆25: 21
26: 21
[18:01:48.184]收←◆27: 21
[18:01:49.211]收←◆21: 81
22: 81
[18:01:49.262]收←◆23: 81
[18:01:49.288]收←◆24: 81
25: 81
26: 81
[18:01:49.367]收←◆27: 81
[18:01:50.393]收←◆21: 81
22: 81
[18:01:50.446]收←◆23: 81
24: 81
[18:01:50.498]收←◆25: 81
[18:01:50.523]收←◆26: 81
27: 81
[18:01:51.577]收←◆21: 81
[18:01:51.603]收←◆22: 81
23: 81
24: 81
[18:01:51.681]收←◆25: 81
26: 81
[18:01:51.733]收←◆27: 81
[18:01:52.759]收←◆21: 81
[18:01:52.786]收←◆22: 81
23: 81
[18:01:52.838]收←◆24: 81
[18:01:52.864]收←◆25: 81
26: 81
[18:01:52.916]收←◆27: 81
[18:01:53.943]收←◆21: 21
22: 21
[18:01:53.996]收←◆23: 21
[18:01:54.021]收←◆24: 21
25: 21
[18:01:54.072]收←◆26: 21
[18:01:54.098]收←◆27: 21
[18:01:55.126]收←◆21: 81
[18:01:55.152]收←◆22: 81
[18:01:55.177]收←◆23: 81
24: 81
[18:01:55.230]收←◆25: 81
[18:01:55.256]收←◆26: 81
27: 81
[18:01:56.308]收←◆21: 81
[18:01:56.335]收←◆22: 81
23: 81
[18:01:56.386]收←◆24: 81
[18:01:56.412]收←◆25: 81
26: 81
[18:01:56.465]收←◆27: 81
[18:01:57.491]收←◆21: 81
22: 81
23: 81
[18:01:57.570]收←◆24: 81
25: 81
[18:01:57.622]收←◆26: 81
[18:01:57.648]收←◆27: 81
[18:01:58.675]收←◆21: 81
[18:01:58.701]收←◆22: 81
[18:01:58.727]收←◆23: 81
24: 81
25: 81
[18:01:58.805]收←◆26: 81
27: 81
[18:01:59.857]收←◆21: 81
[18:01:59.883]收←◆22: 81
23: 81
[18:01:59.936]收←◆24: 81
[18:01:59.962]收←◆25: 81
26: 81
27: 81
[18:02:01.041]收←◆21: 81
[18:02:01.067]收←◆22: 81
23: 81
[18:02:01.118]收←◆24: 81
25: 81
[18:02:01.170]收←◆26: 81
[18:02:01.196]收←◆27: 81
[18:02:02.224]收←◆21: 21
22: 21
[18:02:02.275]收←◆23: 21
[18:02:02.301]收←◆24: 21
25: 21
[18:02:02.354]收←◆26: 21
[18:02:02.379]收←◆27: 21
[18:02:03.406]收←◆21: 81
22: 81
[18:02:03.459]收←◆23: 81
24: 81
[18:02:03.510]收←◆25: 81
[18:02:03.537]收←◆26: 81
27: 81
[18:02:04.589]收←◆21: 81
[18:02:04.615]收←◆22: 81
23: 81
[18:02:04.667]收←◆24: 81
[18:02:04.694]收←◆25: 81
26: 81
[18:02:04.746]收←◆27: 81
[18:02:05.772]收←◆21: 81
22: 81
[18:02:05.825]收←◆23: 81
[18:02:05.850]收←◆24: 81
25: 81
[18:02:05.902]收←◆26: 81
[18:02:05.929]收←◆27: 81
[18:02:06.955]收←◆21: 81
22: 81
[18:02:07.008]收←◆23: 81
24: 81
[18:02:07.060]收←◆25: 81
[18:02:07.086]收←◆26: 81
27: 81
[18:02:08.139]收←◆21: 81
[18:02:08.165]收←◆22: 81
23: 81
24: 81
[18:02:08.242]收←◆25: 81
26: 81
[18:02:08.294]收←◆27: 81
[18:02:09.321]收←◆21: 81
22: 81
[18:02:09.374]收←◆23: 81
[18:02:09.399]收←◆24: 81
25: 81
26: 81
[18:02:09.478]收←◆27: 81
[18:02:10.505]收←◆21: 81
22: 81
[18:02:10.555]收←◆23: 81
[18:02:10.583]收←◆24: 81
25: 81
[18:02:10.634]收←◆26: 81
27: 81
[18:02:11.687]收←◆21: 81
[18:02:11.713]收←◆22: 81
[18:02:11.739]收←◆23: 81
24: 81
[18:02:11.791]收←◆25: 81
[18:02:11.818]收←◆26: 81
27: 81
[18:02:12.870]收←◆21: 81
[18:02:12.896]收←◆22: 81
23: 81
[18:02:12.949]收←◆24: 81
[18:02:12.974]收←◆25: 81
26: 81
[18:02:13.026]收←◆27: 81
[18:02:14.053]收←◆21: 81
22: 81
[18:02:14.105]收←◆23: 81
[18:02:14.131]收←◆24: 81
25: 81
[18:02:14.184]收←◆26: 81
[18:02:14.209]收←◆27: 81
[18:02:15.236]收←◆21: 81
22: 81
[18:02:15.289]收←◆23: 81
24: 81
25: 81
[18:02:15.366]收←◆26: 81
27: 81
[18:02:16.420]收←◆21: 81
[18:02:16.445]收←◆22: 81
23: 81
[18:02:16.497]收←◆24: 81
[18:02:16.523]收←◆25: 81
26: 81
27: 81
[18:02:17.603]收←◆21: 81
22: 81
[18:02:17.654]收←◆23: 81
[18:02:17.680]收←◆24: 81
25: 81
[18:02:17.732]收←◆26: 81
[18:02:17.758]收←◆27: 81
[18:02:18.785]收←◆21: 81
22: 81
[18:02:18.837]收←◆23: 81
24: 81
25: 81
[18:02:18.915]收←◆26: 81
[18:02:18.942]收←◆27: 81
[18:02:19.968]收←◆21: 81
[18:02:19.994]收←◆22: 81
[18:02:20.020]收←◆23: 81
24: 81
[18:02:20.072]收←◆25: 81
[18:02:20.098]收←◆26: 81
27: 81
[18:02:21.151]收←◆21: 81
[18:02:21.177]收←◆22: 81
23: 81
[18:02:21.229]收←◆24: 81
[18:02:21.255]收←◆25: 81
26: 81
[18:02:21.307]收←◆27: 81
[18:02:22.334]收←◆21: 81
22: 81
[18:02:22.387]收←◆23: 81
[18:02:22.413]收←◆24: 81
25: 81
[18:02:22.464]收←◆26: 81
[18:02:22.489]收←◆27: 81
[18:02:23.518]收←◆21: 81
[18:02:23.543]收←◆22: 81
[18:02:23.569]收←◆23: 81
24: 81
[18:02:23.621]收←◆25: 81
[18:02:23.647]收←◆26: 81
27: 81
[18:02:24.701]收←◆21: 81
[18:02:24.726]收←◆22: 81
23: 81
[18:02:24.778]收←◆24: 81
[18:02:24.803]收←◆25: 81
26: 81
[18:02:24.856]收←◆27: 81
[18:02:25.883]收←◆21: 81
22: 81
23: 81
[18:02:25.961]收←◆24: 81
25: 81
26: 81
[18:02:26.039]收←◆27: 81
[18:02:27.066]收←◆21: 81
[18:02:27.092]收←◆22: 81
[18:02:27.118]收←◆23: 81
24: 81
25: 81
[18:02:27.196]收←◆26: 81
27: 81
[18:02:28.249]收←◆21: 81
[18:02:28.275]收←◆22: 81
[18:02:28.301]收←◆23: 81
24: 81
[18:02:28.353]收←◆25: 81
26: 81
27: 81
[18:02:29.432]收←◆21: 81
[18:02:29.458]收←◆22: 81
23: 81
[18:02:29.511]收←◆24: 81
[18:02:29.536]收←◆25: 81
26: 81
[18:02:29.587]收←◆27: 81
[18:02:30.616]收←◆21: 81
22: 81
[18:02:30.666]收←◆23: 81
[18:02:30.693]收←◆24: 81
25: 81
[18:02:30.745]收←◆26: 81
[18:02:30.771]收←◆27: 81
[18:02:31.797]收←◆21: 81
22: 81
[18:02:31.850]收←◆23: 81
24: 81
[18:02:31.902]收←◆25: 81
[18:02:31.927]收←◆26: 81
27: 81
[18:02:32.981]收←◆21: 81
[18:02:33.006]收←◆22: 81
23: 81
[18:02:33.059]收←◆24: 81
[18:02:33.085]收←◆25: 81
26: 81
27: 81
[18:02:34.164]收←◆21: 81
22: 81
[18:02:34.216]收←◆23: 81
[18:02:34.242]收←◆24: 81
25: 81
26: 81
[18:02:34.320]收←◆27: 81
[18:02:35.347]收←◆21: 81
[18:02:35.372]收←◆22: 81
[18:02:35.399]收←◆23: 81
24: 81
[18:02:35.451]收←◆25: 81
[18:02:35.477]收←◆26: 81
27: 81
[18:02:36.530]收←◆21: 81
[18:02:36.556]收←◆22: 81
23: 81
24: 81
[18:02:36.634]收←◆25: 81
26: 81
[18:02:36.685]收←◆27: 81
[18:02:37.714]收←◆21: 21
[18:02:37.739]收←◆22: 21
23: 21
[18:02:37.790]收←◆24: 21
25: 21
26: 21
[18:02:37.869]收←◆27: 21
[18:02:38.895]收←◆21: 81
22: 81
[18:02:38.948]收←◆23: 81
[18:02:38.974]收←◆24: 81
25: 81
[18:02:39.025]收←◆26: 81
[18:02:39.051]收←◆27: 81
[18:02:40.078]收←◆21: 81
22: 81
[18:02:40.130]收←◆23: 81
24: 81
[18:02:40.183]收←◆25: 81
[18:02:40.209]收←◆26: 81
27: 81
[18:02:41.261]收←◆21: 81
[18:02:41.288]收←◆22: 81
23: 81
[18:02:41.340]收←◆24: 81
[18:02:41.366]收←◆25: 81
26: 81
27: 81
[18:02:42.445]收←◆21: 81
22: 81
23: 81
[18:02:42.523]收←◆24: 81
25: 81
[18:02:42.575]收←◆26: 81
[18:02:42.601]收←◆27: 81
[18:02:43.628]收←◆21: 21
[18:02:43.654]收←◆22: 21
[18:02:43.680]收←◆23: 21
24: 21
25: 21
[18:02:43.758]收←◆26: 21
27: 21
[18:02:44.811]收←◆21: 81
[18:02:44.837]收←◆22: 81
23: 81
[18:02:44.889]收←◆24: 81
[18:02:44.914]收←◆25: 81
26: 81
27: 81
[18:02:45.994]收←◆21: 81
22: 81
23: 81
[18:02:46.071]收←◆24: 81
[18:02:46.098]收←◆25: 81
26: 81
[18:02:46.149]收←◆27: 81
[18:02:47.177]收←◆21: 81
22: 81
[18:02:47.228]收←◆23: 81
[18:02:47.254]收←◆24: 81
25: 81
[18:02:47.307]收←◆26: 81
[18:02:47.333]收←◆27: 81
[18:02:48.359]收←◆21: 81
[18:02:48.385]收←◆22: 81
[18:02:48.412]收←◆23: 81
24: 81
[18:02:48.464]收←◆25: 81
[18:02:48.490]收←◆26: 81
27: 81
[18:02:49.543]收←◆21: 81
[18:02:49.569]收←◆22: 81
23: 81
[18:02:49.621]收←◆24: 81
[18:02:49.647]收←◆25: 81
26: 81
[18:02:49.699]收←◆27: 81
[18:02:50.725]收←◆21: 81
22: 81
[18:02:50.778]收←◆23: 81
[18:02:50.804]收←◆24: 81
25: 81
26: 81
[18:02:50.882]收←◆27: 81
[18:02:51.909]收←◆21: 81
[18:02:51.935]收←◆22: 81
[18:02:51.962]收←◆23: 81
24: 81
[18:02:52.013]收←◆25: 81
[18:02:52.038]收←◆26: 81
27: 81
[18:02:53.092]收←◆21: 21
[18:02:53.118]收←◆22: 21
23: 21
24: 21
[18:02:53.196]收←◆25: 21
26: 21
[18:02:53.248]收←◆27: 21
[18:02:54.274]收←◆21: 81
[18:02:54.301]收←◆22: 81
23: 81
[18:02:54.352]收←◆24: 81
25: 81
26: 81
[18:02:54.431]收←◆27: 81
[18:02:55.457]收←◆21: 21
22: 21
[18:02:55.509]收←◆23: 21
[18:02:55.536]收←◆24: 21
25: 21
[18:02:55.588]收←◆26: 21
[18:02:55.614]收←◆27: 21
[18:02:56.640]收←◆21: 81
[18:02:56.667]收←◆22: 81
[18:02:56.693]收←◆23: 81
24: 81
[18:02:56.744]收←◆25: 81
[18:02:56.771]收←◆26: 81
27: 81
[18:02:57.823]收←◆21: 81
[18:02:57.850]收←◆22: 81
23: 81
[18:02:57.902]收←◆24: 81
[18:02:57.928]收←◆25: 81
26: 81
[18:02:57.980]收←◆27: 81
[18:02:59.007]收←◆21: 81
22: 81
[18:02:59.058]收←◆23: 81
[18:02:59.085]收←◆24: 81
25: 81
[18:02:59.136]收←◆26: 81
[18:02:59.162]收←◆27: 81
[18:03:00.190]收←◆21: 81
[18:03:00.216]收←◆22: 81
[18:03:00.241]收←◆23: 81
24: 81
25: 81
[18:03:00.320]收←◆26: 81
27: 81
[18:03:01.372]收←◆21: 81
[18:03:01.398]收←◆22: 81
23: 81
[18:03:01.450]收←◆24: 81
[18:03:01.476]收←◆25: 81
26: 81
27: 81
[18:03:02.555]收←◆21: 81
22: 81
23: 81
[18:03:02.633]收←◆24: 81
25: 81
[18:03:02.686]收←◆26: 81
[18:03:02.712]收←◆27: 81
[18:03:03.739]收←◆21: 81
22: 81
[18:03:03.791]收←◆23: 81
24: 81
25: 81
[18:03:03.868]收←◆26: 81
[18:03:03.895]收←◆27: 81
[18:03:04.921]收←◆21: 21
[18:03:04.947]收←◆22: 21
[18:03:04.974]收←◆23: 21
24: 21
[18:03:05.025]收←◆25: 21
[18:03:05.052]收←◆26: 21
27: 21
[18:03:06.105]收←◆21: 81
[18:03:06.131]收←◆22: 81
23: 81
[18:03:06.182]收←◆24: 81
[18:03:06.209]收←◆25: 81
26: 81
[18:03:06.260]收←◆27: 81
[18:03:07.287]收←◆21: 21
22: 21
[18:03:07.340]收←◆23: 21
[18:03:07.365]收←◆24: 21
25: 21
[18:03:07.417]收←◆26: 21
[18:03:07.444]收←◆27: 21
[18:03:08.470]收←◆21: 81
22: 81
[18:03:08.522]收←◆23: 81
24: 81
[18:03:08.574]收←◆25: 81
[18:03:08.600]收←◆26: 81
27: 81
[18:03:09.653]收←◆21: 81
[18:03:09.679]收←◆22: 81
23: 81
24: 81
[18:03:09.757]收←◆25: 81
26: 81
[18:03:09.810]收←◆27: 81
[18:03:10.836]收←◆21: 21
22: 21
[18:03:10.889]收←◆23: 21
[18:03:10.915]收←◆24: 21
25: 21
26: 21
[18:03:10.992]收←◆27: 21
[18:03:12.019]收←◆21: 81
[18:03:12.045]收←◆22: 81
[18:03:12.071]收←◆23: 81
24: 81
[18:03:12.124]收←◆25: 81
[18:03:12.150]收←◆26: 81
27: 81
[18:03:13.203]收←◆21: 81
[18:03:13.229]收←◆22: 81
[18:03:13.255]收←◆23: 81
24: 81
[18:03:13.306]收←◆25: 81
[18:03:13.332]收←◆26: 81
27: 81
[18:03:14.385]收←◆21: 81
[18:03:14.411]收←◆22: 81
23: 81
[18:03:14.463]收←◆24: 81
[18:03:14.489]收←◆25: 81
26: 81
[18:03:14.541]收←◆27: 81
[18:03:15.569]收←◆21: 81
22: 81
[18:03:15.620]收←◆23: 81
[18:03:15.646]收←◆24: 81
25: 81
[18:03:15.698]收←◆26: 81
[18:03:15.724]收←◆27: 81
[18:03:16.751]收←◆21: 81
[18:03:16.777]收←◆22: 81
[18:03:16.803]收←◆23: 81
24: 81
[18:03:16.855]收←◆25: 81
[18:03:16.881]收←◆26: 81
27: 81
[18:03:17.934]收←◆21: 81
[18:03:17.960]收←◆22: 81
23: 81
[18:03:18.013]收←◆24: 81
[18:03:18.038]收←◆25: 81
26: 81
27: 81
[18:03:19.117]收←◆21: 81
22: 81
23: 81
[18:03:19.195]收←◆24: 81
25: 81
[18:03:19.248]收←◆26: 81
[18:03:19.273]收←◆27: 81
[18:03:20.300]收←◆21: 81
22: 81
[18:03:20.353]收←◆23: 81
24: 81
[18:03:20.404]收←◆25: 81
[18:03:20.430]收←◆26: 81
27: 81
[18:03:21.483]收←◆21: 21
22: 21
23: 21
24: 21
[18:03:21.587]收←◆25: 21
26: 21
27: 21
[18:03:22.667]收←◆21: 81
[18:03:22.692]收←◆22: 81
23: 81
[18:03:22.744]收←◆24: 81
25: 81
26: 81
[18:03:22.822]收←◆27: 81
[18:03:23.848]收←◆21: 81
示波器测量的位置与波形记录如下:



您好
现在我已经浏览了你们的原理图、看到 BTST 二极管是普通二极管。 BTST 二极管(D4和 D5)需要为肖特基二极管、以便反向恢复电荷较少。
我还为原理图提供了一些建议:
我建议将一个小型陶瓷电容器与 C34并联。 这将有助于滤除由 Q7引起的高频开关噪声。 我建议在 VBAT 侧用 C27做同样的事情。
我建议将 RC 滤波器与 ICHG 电阻器并联安装。 因此、我们建议使用大于5kΩ 的电阻器。
我还有一些关于布局的建议:
HIDRV、LODRV 和 SW 布线需要至少为20mil。
SW 是 HIDRV 的返回路径。 确保将 SW1/SW2连接到 HIDRV1/HIDRV2旁边。
GND 是 LODRV 的返回路径。 确保 LODRV 在 GND 布线或平面旁边布线。
我认为替换 BTST 二极管将对电路性能产生最主要的影响。 如果有需要、请告诉我。
如果同时还有其他问题、请告诉我。