要求电路简单,电压设定精度高,欠压门限可调(暂定8V)。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
以下两种方案,你可以考虑一下,但是前提是,你的设计里面是否可以带MCU控制?
1、比较器+MCU控制:最简单的比较器电路,可以用LM393之类的,然后通过设定门限值,即你暂定的8V,考虑到器件的差异性,建议留余量设计。将比较结果(电平信号)输入到MCU的IO口,IO口监测发现电池(假定是)电压低或者高于8V的时候,控制LED输出不同的状态显示,闪烁的效果,可以通过控制占空比完成,然后占空比可调(便于后续增加诸如慢闪、中闪、快闪等不同状态)。该方案的特点是比较精确,缺点是成本相对较高,且调试时会费时。
2、采样电阻+MCU控制:相对简单,将电压接入到采样电阻中,同样将该信号接入到MCU的IO口进行监测,其他与方案1相似。优点是,简单、成本便宜,缺点是不精确。