This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138064无法再次烧录,无法转ROM模式

Other Parts Discussed in Thread: UCD3138, UCD3138064EVM-166, UCD3138064

手上的UCD3138064EVM-166不小心错烧录了UCD3138的程序,因为校验和是对的,所以上电后直接从BOOT ROM转到FLASH,但是FLASH的程序又不能正常运行,所以无法再次转BOOT ROM。

前段时间恰好看到应用文章“ 如何防止 UCD3138无法再次烧录”,文中提到出现这种情况“如果 PMBus 不能正常通信,这时可以将Fault 3 引脚接低电平,再复位芯片,这样也可以回到ROM 模式”。但是尝试很多次仍不能回到ROM模式。

想问一下,除了要将Fault 3 引脚接低电平,再复位芯片,还有其它要注意的吗?还是这个方法只适用UCD3138,对UCD3138064不适用?