This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM22676和TPS5430性能上对比有什么区别?
能否告知你是想应用在哪些方面?对输入电压、输出电压及电流的要求是什么?
你指的应该是LM2676吧。
其实国半的LM2676和TPS5430都是开关电源芯片,性能区别在以下:
指标 LM2676 TPS5430
输入电压 8-40V 5.5-36V
输出电流 3A 3A
最高效率 94% 95%
内置mos 150 mΩ 110 mΩ
开关频率 260KHz 500KHz (选电感会小一些)
输出电压精度 2% 1.5%