This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: 如何设置电池充满的条件

Part Number: BQ40Z80


你好,

我现在一个电池包的应用是7S1P, 电芯是18650锂离子电池,2500mAh。目前的设置是:当每节电芯的电压大于4.1时,并且电流小于150mAh, SOC一段时间稳定不变,BQ40Z80会终止充电,并且对FC(Fully charged)标志位置位。在另外一种充电情况下,电池包会停止充电,但是不会对FC置位:当某单节电池达到4.19V(4.19V被设置为电压过充的门槛),BMS会终止充电。

电池工程师说:在计算SOC时,FC有没有置位,算法是不同的。FC置位的情况下,产品应用端的表现会比较正常。但是在FC不置位而结束充电的情况下,产品应用端电池包的SOC偶尔会出现异常。实际上,主要的问题可能是电池的内阻较大,在完成若干次充放电后,单个电芯之间内阻和压差增大。在某种情况下,充电电流还远大于150mA时,某节电芯的电压以及达到了过压门槛4.19V,从而触发了终结充电。但是FC是没有置位的。而是看到DSG被置位。

我的问题是:

是否可以将终止充电并置位的条件从当前的:当每节电芯的电压大于4.1时,并且电流小于150mAh, SOC一段时间稳定不变,BQ40Z80会终止充电,并且对FC(Fully charged)标志位置位。

改为:当每节电芯的电压大于4.1时,并且满足下面2个条件中的1个条件,BQ40Z80终止充电,并且对FC标志位置位。

1. 电流小于150mAh, SOC一段时间稳定不变。

2. 某节电池电压达到4.19V。

Regards

Alex Chen