This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV752: Related issues with current output

Part Number: TLV752


hello everyone!

Can this electronic component output 1A for each channel?

Or can two channels combined output 1A?

My usage scenario is that there is only one channel in use.I didn't see it clearly in the datasheet...