This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 温度模型

Part Number: BQ76952


Dears,

我们正在参考TI 文档ZHCABZ9做不同型号NTC得温度采样,用到了两个不同的NTC,分别使用用TS1和TS2,采样都配置为上拉10KΩ,在采用18KΩ的时候,温度能正确读出来,采用180KΩ的模型时,得到的温度不正确,采用自己的温度模型时,温度也能读出来,配置如下,目前未注释掉的是用18KΩ模型的代码,可以读到正确的温度数据;想请教下在同一系统中使用两种不同NTC,在上拉电阻都选择18KΩ上拉情况下,同时使用内部18KΩ和180KΩ的温度模型应该怎么配置,目前看文档里面说是支持的,希望得到解答,谢谢

zhcabz9.pdf