Other Parts Discussed in Thread: LM61460
各位好,
我打算使用lmr51450作为typec pd的电源供电端,可以上电状态下,根据pdo设置,输出5/9/12/15/20v的电源,下面是我参照ti其他器件的开发板设计的原理图

请问lmr51450是否可以这样使用?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你能告诉我们每个输出电压设置的输出电流水平吗?我们需要看到,对于给定的输出电压/电流设置,在固定电感器和输出电容器的情况下,系统能否稳定,并具有足够的增益和相位裕度。
只需注意一点,您可能需要考虑将FET V39移动到V42作为接地参考,因为这样更容易驱动。
我刚刚为不同的VOUT/IOUT设置运行了快速启动计算器,我发现在给定的输出条件下,相位裕度不足以确保该转换器的稳定运行。
当我说FET需要接地时,我的意思是将FET源极连接到GND,并将低压侧反馈电阻器移动到漏极侧(只需交换FET和反馈电阻器的位置)。希望这是清楚的。
您可以查看LM61460数据表应用部分,其中有USB Type C应用示意图。请参阅第9.2.4节USB Type-C系统示例。这与您的系统用例非常接近。