This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195可以正常充电,但是升压电压带不动负载,且电压为6点几伏

Other Parts Discussed in Thread: BQ24195

BQ24195可以正常充电,但是升压电压带不动负载,且电压为6点几伏(电池电压为4.1伏),一接负载电压就掉到1.7伏左右。我的升压寄存器配置是。

BQ24195_Write_Byte(0x00,0x37);
BQ24195_Write_Byte(0x01,0x2b); // Éýѹ
BQ24195_Write_Byte(0x02,0xf0);
BQ24195_Write_Byte(0x03,0x11); // ³äµçµçÁ÷ÉèÖÃ
BQ24195_Write_Byte(0x05,0x8A); // II2¿´ÃŹ·

  • 刚才做了测试,我的升压输出,会根据负载大小变化。没接负载升压后的电压是11.2V,接入USB电流电压检测器,看到的电压是10.3V;用小风扇测试用USB检测器看电压,电压掉到4.53V此时电流为160mA;直接给手机供电,用USB检测器看电压,电压掉到4.5V以下。

  • 标题中的正常充电是指可以给电池大电流充电。现在换了一个二极管SS14(在PMID和SW脚之间)电压由之前的6点几直接飞到11点几伏。Ps,之前的二极管不知道型号。

  • BQ24195在boost 模式下,只有5V左右的电压,如果看到11.2V,显然是不在正常工作。建议观察下开关波形,看看是否不是正常的方波。如果芯片不在正常工作,也无所谓带不带的动负载。需要找出为什么不能正常输出。建议你看下PCB layout,PMID-cap-IC GND这个回路是否很长。REGN的电容是否远离芯片。