This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高温降压使用,充电过程中RSOC跳变

Other Parts Discussed in Thread: BQ28Z610-R1

BQ28Z610-R1设置了高温降压充电,在0~45℃下满充电压为8.648V,在45~60℃满充电压为8.4V。

电池在30℃时候开始用8.648V,5A进行充电,一段时间后电池温度开始上升,当电池达到46℃的时候,RSOC为70%,此时开始降压充电,充电器开始降到8.4V,1152mA的电流去给电池充电,但是当充到91%就达到了满充截止条件,此时RSOC从91%直接跳变到100%,请问是否有方法让RSOC不跳变,而是平滑到100%?