目前我们使用PWM信号的电源芯片,通过调节占空比、配置外部电阻实现将3.3V电压转化为0~3.3V的多种电压档位输出。由于所需要的输出电压比较多(最高达到80路),需要使用非常多的RC电路。
所以想咨询下有没有集成的方案:
1、是否有集成的输出档位可选/可调的芯片?要求输出可以在0~3.3V内有多个档位可选
2、是否有集成多路RC网络的(RC组合)的芯片?可以通过输入PWM信号进行输出可调在0~3.3V内?
或者有其他可以实现的方案也可以推荐下,谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.