This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NI-MH充放电



大神们:
          我手上有个LED的手电筒,输入是+12V的,接的是4个NI-MH纽扣电池串联起来的NI-MH电池,现在我有几个疑问

           1  为什么当我把+12V的电源给NI-MH电池充电,充电电流非常少,只有几十毫安。

           2   NI-MH的输出电流有什么特点?好像NI-MH输出电流都很弱,也就只有10毫安,

           3   有IC推荐 或者相关的NI-MH的资料吗  ?

     谢谢

  • 充电需要恒流充电, 请问适配器的输出特性如何。 

    另外 如果电池电压过高,也会造成电流过小

    NiMH容量密度小, 有记忆效应, 电池输出能力这个要看电池的容量,确实是比锂电池小