This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: WEBENCH设计原理图带不动负载,输入电流不超过20mA

Part Number: UCC28740

我根据WEBENCH内的设计,制作了一款输入110V输出24V的反激式开关电源,设计之初考虑为48W功率(变压器似乎没有问题),目前的情况是只能带动1W左右的功率(110V电压 12mA电流),如果加负载则出现类似重启的情况,表现为110V输入电压掉压为50-80V,电流始终不能超过20mA,感觉触发了芯片的过流保护,请问是否为该芯片UCC28740的过流保护?设计严格按照WEBENCH里的原理图,如果是我该如何改正,如果不是我该如何排除问题?

原理图:

变压器参数:

PI-103725-00 EDA.pdf

现象视频:

麻烦能解答一下问题的原因,不胜感激。