BQ79616电池管理芯片,最多可以多少个芯片叠加,最大电压可以做到2500V吗?两通道之间耐压可以做到200VAC吗?如果我监测电芯电压,而监测的电芯不是连续串联的,有什么好的方案可以说一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
假设每个电池为4V,每个616监测16个电池,则需要40个BQ79616设备。这将得到支持,因为616最多可以堆叠64x BQ79616设备。200VAC从哪里来?它所应用的两通道在哪里?施加200VAC的时间有多长?
只要连接到每个BQ79616的单元是连续的,这是可以的,但这些单元在BQ79616设备之间没有连接。可以将所有这些电池模块的接地平面连接在一起,因为没有模块与另一个电池模块串联。只要没有模块与属于另一个BQ79616设备的另一个模块串联,就可以不连接接地平面或连接接地面。