Dear Sir/Madam,
We have currently provided you with the schematic attachment of the TPS53667RTAR and 6 CSD95490Q5MCs, and we are aiming to implement the buck output of a 6-phase interleaved parallel buck circuit, but while editing using the Fusion Design Online software, we would like to select the 6-phase phase-shifted output, but we will get a popup of the ‘wrote Six Phase [0x05] to the device and it was ACKed, but a write verification read back returned One Phase [0x00]’. To make sure if the TPS53667RTAR chip has been set up for 6 phase output, if it has not been set up successfully, what is the reason for the failure.