请问该芯片充电的时候PWM占空比是用什么来控制的,充电电流大小和开关频率之间有没有什么计算公式。我想要得到2A的充电电流,但是不知道从哪里去控制
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问该芯片充电的时候PWM占空比是用什么来控制的,充电电流大小和开关频率之间有没有什么计算公式。我想要得到2A的充电电流,但是不知道从哪里去控制
你好,你所指的2A是快速充电时的电流吗?
如果是的话,充电电流可以通过公式6
(datashe的第12页)来调节电流的大小。
开关频率的大小与PIN9的TPWM与PIN12的VSS之间的外接电容的大小有关。参考公式7进行设置。
另外PWM占空比的大小是芯片内部自己调节的:可通过SNS引脚和BAT引脚分别对充电电流和充电电压进行监控,将检测信号与内置阈值进行比较后,器件将通过MOD引脚输出PWM控制信号,以维持电流或电压的恒定,该PWM控制信号的最大占空比为80%。
另外请访问:http://www.ti.com/product/bq2954
里面有详细的datasheet和applications notes.