This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B86-Q1: Load transient

Part Number: TPS7B86-Q1

TPS7B8633BQ这款芯片的load transient特性,是否有VOUT = 3.3 V, IOUT = 0 mA to 375 mA, slew rate = 0.1 A/µs条件的数据,或者近似数据也可以。

(TI网站上找到的datasheet中slew rate=0.1A/us对应的IOUT变动数值都比较小,而我们实际使用的IOUT变动比较大。)