您好!
我们在做铅酸电池充电器,请问贵司的BQ24610电池充电管理芯片的充电电流可不可以设置到20A,甚至30A?
从数据手册上下面的公式应该是可以的,Rsr选10毫欧充电电流是10A,如果选5毫欧,充电电流是不是就能达到20A? 但是数据手册上写该芯片的最大充电电流是10A。
期待回复,谢谢!
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.