在芯片手册里有这么一句话,如果需要在PMID上获得5V的电压,需要按下面的设置来设置
我上电就给了OTG pin一个高电平,然后REG01写入了0x54,但是我在PMID得不到5V,只有3.7V。
这个时候我按下S1按钮后,指示灯(原理图图片中没有)闪一下,立刻就灭掉了,而且PMID的电压用示波器看越来越小,直到变为1V左右。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1, BOOST 如果没有工作,PMID脚上看到的电压等于(接近)电池电压。
2. 在REG01中写入0x54,即01010100,对应的bit5和bit4是01,不是要求的10,自然无法进入boost mode。(注意最左边一位是bit0)另外,bit0也应该为1.
请参阅datasheet的REG01配置描述部分。