This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

推荐可连续调节的升压芯片



Hi, 各位专家

      我们需要设计一款DC-DC 升压电源,具体要求如下:

(1)输入电压范围4.5VDC~13.5VDC

(2)能外接一个电位器调节输出电压;

(3)输出电压范围为5VDC~14VDC.

(4)最大输出电流:大于或等于3A

         我们其实需要两个通道,一个通道是把5VDC输入电压升压到6V左右输出,另一个通道是把12VDC输入电压升压到13V左右输出。如果两个通道不能使用同一个芯片,也可以考虑两个通道使用不同的芯片。

        麻烦各位给出建议,谢谢!