This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ500215问题咨询

Other Parts Discussed in Thread: BQ500215, BQ51025, CSD97374Q4M

Hi:

       TI工程师

       我有几个关于BQ500215的问题:

1.BQ500215电压输入范围必须是12V左右,如果我的BQ51025设置为5V 2A模式,BQ500215是否可以降低电压。

2.BQ500215的datasheet好像没有提供debug方面的信息。我如果只是简单的作为无线充电发射端,芯片的默认寄存器设置是否能够输出5V2A,或者10V 1A

3.从照片上看BQ500215demo板上,是否有一条蓝色的飞线。如果是,官方的原理图和PCB图上是否已经更正?

4.BQ500215配合的CSD97374Q4M 是否还有其他型号备选?

        谢谢

  • 1.BQ500215电压输入范围必须是12V左右,如果我的BQ51025设置为5V 2A模式,BQ500215是否可以降低电压。

    --BQ500215是为12V输入设计。不建议用在5V输入应用。

    2.BQ500215的datasheet好像没有提供debug方面的信息。我如果只是简单的作为无线充电发射端,芯片的默认寄存器设置是否能够输出5V2A,或者10V 1A

    ---在发射端本身只提供功率而没有直接的电压输出,输出端电压发生在接受端,由线圈和接收端设置决定。

    3.从照片上看BQ500215demo板上,是否有一条蓝色的飞线。如果是,官方的原理图和PCB图上是否已经更正?

    4.BQ500215配合的CSD97374Q4M 是否还有其他型号备选

    ---理论上可以选用其他型号。但TI的Demo上选用该MOS,并经过测试,能通过WPC认证,建议完全follow该设计。