Part Number: LM27762
Hi,最近在使用LM27762,采用了3.3V转±1.8V的方式。±1.8V是用于给ADC芯片(AD7124)供电使用,ADC规格书中描述最大功率需要的电流约1mA左右
±1.8V仅用于该ADC,也就是说负载电流仅1mA,属于非常小的负载了。想问一下这种情况下,芯片的转换效率能有多少,规格书中只给出了-5V的转换效率
感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM27762
Hi,最近在使用LM27762,采用了3.3V转±1.8V的方式。±1.8V是用于给ADC芯片(AD7124)供电使用,ADC规格书中描述最大功率需要的电流约1mA左右
±1.8V仅用于该ADC,也就是说负载电流仅1mA,属于非常小的负载了。想问一下这种情况下,芯片的转换效率能有多少,规格书中只给出了-5V的转换效率
感谢
您好,
对于数据手册中未提供的效率信息,通常可使用webench设计并评估其效率。
LM27762没有相关数据,效率=输出功率/(输出功率+耗散功率)
耗散功率计算请参考芯片数据手册8.2.2.6 Power Dissipation.
下面帖子讨论了类似问题,请参考。