Other Parts Discussed in Thread: BQ25188, BQ25185
各位好,我对TI的BQ24030芯片有一些疑惑,因为我个人接触硬件不是很久,也麻烦大家可以解答我以下问题:
(1)BQ24030的AC引脚是否可以接入太阳能板进行供电,如果可以,其输出电压范围是否在4.35V~16V之间、100mA~2A之间?接入太阳能板的话要怎么让太阳能板达到类似MPPT的功能?
(2)对于芯片上的USB引脚是否可以由我直接画的PCB上接入的TYPEC进行5V供电,我再直接对芯片设置500mA的USB限制电流?
(3)芯片上的一些状态引脚是否可以直接悬空,例如引脚USBPG、ACPG以及TMR、LDO、TS在不使用这些功能时是否可以直接悬空?
(4)对于OUT引脚的输出电压是如何计算的?如果后续电路的IC芯片都是需要3V3的工作电压,我是否最好再加一个BUCK-BOOST电路进行稳压?
(5)我的使用场景是对传感器节点进行供电,其中节点模块携带有单节电池,并通过TYPEC和太阳能进行充电,TYPEC输入为主要的电池充电电源,这种场景下用这款芯片应该没问题吧?或者有没有其他更好的选择