This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750EVM: BQ25731

Part Number: TPS25750EVM
Other Parts Discussed in Thread: BQ25731,

Hi Ti Team

If I use Type-C input voltage (PD Max 100W), will it use BATT (TP3) as the output?

Can I pin out a wire from the TP3 pin and charge a device, such as a tablet or laptop?

If it is Default's TPS25750EVM, what is the voltage range that BQ25731 can output?

Is it adjusted according to the picture below? or I need to rewrite the firmware using the GUI?