Other Parts Discussed in Thread: TPS25751
Regarding the power supply negotiation issue, the following questions exist:
1. When a charging adapter supporting the PD protocol is input, the TPS25730 should be able to recognize it. After a successful negotiation, the currently negotiated voltage and operational current with the charging adapter should be written into the TX_SINK_CAPS Register. In this way, the external MCU can obtain the power supply capabilities (including voltage and current capabilities) of the current charging adapter through I2C. Is the above understanding correct?
2. For a charging adapter that does not support the PD protocol (such as 5V 1A), can the TPS25730 recognize the charging capabilities (voltage and current) of the charging adapter? Can it supply power normally? If it can recognize and supply power, can the external MCU obtain this part of the information?
Circuit configuration: 1. Is it necessary to connect an external power supply to VIN_3V3? Can the TPS25730 operate normally if it is not connected? It seems that there is no connection on the EVM development board.