Hello,我们的一个板子上使用LM2936Z-5.0/NOPB,但发现这个LDO输出值有异常。不同的批次输出值有差别,有的可以输出很稳定的5V,如5.023V;但是也存在其他批次,输出值偏高,我特别从TI申请了样片,也存在此问题,可达到5.544V,远超出元件的规格。
电路上,5V输出用于给光耦HCLP7840的VDD1供电,从光耦的规格书看,IDD1的典型功耗是10.86mA,符合LDO的供电范围。电源输入值为24.83V。

麻烦看看是什么原因?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.