采用TLV61048,输入电压为3.3V,输出为5V,9V、12V,根据datasheet R1选择为698K,然后选通不同电路输出三种不同电压,经过测试发现,板子刚上电输出正常,然后电压会逐步降低,12V会降到11.5V左右,9V会降到8.65V左右,5V会降到4.9V左右;调整L4电感,或更改电阻后,也是会出现刚上电瞬间工作电压正常,然后电压降低的现象,造成此问题的原因可能是什么?麻烦帮忙看一下原理图设计是否合理,有需要优化的地方?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.