This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: 用TPS5430做负压12V输出时,低频100Hz底噪纹波高出很多,不良率有10%

Part Number: TPS5430


我用TPS5430来设计功放时,同一批次的TPS5430做负压12V输出时,低频100Hz底噪高出很多。正负压都是用的5430

正常的5430在现有的输出上额外挂1.7W负载工作都是正常的,不会出现100Hz频点处凸起

现在一批货,不是所有芯片都有这个问题,有10%出现这种问题,(货绝对是原装)现在不知道怎么去处理这个问题。

电源不是适配器输入,是恒流恒压开关电源输入。

请帮忙分析一下,