Part Number: BQ77216

采用如图电路设计,使用BQ7721612芯片。发现:
1、部分芯片焊接到PCB后接上电池工作正常,部分芯片不断输出报警。
2、有问题芯片,仅从C17_PWR供电50V的情况下,COUT输出高电平7V,DOUT输出低电平。工作正常的芯片,两个脚都输出低电平。
这个现象是电路中有哪个位置设计有问题导致的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ77216

采用如图电路设计,使用BQ7721612芯片。发现:
1、部分芯片焊接到PCB后接上电池工作正常,部分芯片不断输出报警。
2、有问题芯片,仅从C17_PWR供电50V的情况下,COUT输出高电平7V,DOUT输出低电平。工作正常的芯片,两个脚都输出低电平。
这个现象是电路中有哪个位置设计有问题导致的?
您好
根据您提供的资料应该是触发overvoltage
In the BQ77216 device, each cell is monitored independently. Overvoltage is detected by comparing the actual cell voltage to a protection voltage reference, VOV. If any cell voltage exceeds the programmed OV value, a timer circuit is activated. When the timer expires, the COUT pin goes from inactive to active state. The timer is reset if the cell voltage falls below the recovery threshold (VOV – VOV_HYS). Undervoltage is detected by comparing the actual cell voltage to a protection voltage reference, VUV. If any cell voltage falls below the programmed UV value, a timer circuit is activated. When the timer expires, the DOUT pin goes from inactive to active state. The timer is reset if the cell voltage rises below the recovery threshold (VUV + VUV_HYS)
关于如何修改,应该是部分匹配出了问题导致触发过压保护。
Figure 8-1. Timing for Overvoltage Sensing
参考datasheet如图做相关相关电压或者相关匹配调整避免触发造成问题发生。