This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561-R2: 芯片推荐

Part Number: BQ27Z561-R2


你好,

如下需求请帮忙推荐TI的芯片。

18650电池2节并联,带IC保护板,6000mAh

  1. 充电电流2A
  2. 支持i2c读取(或者单独ADCMCU只剩下单路ADC可用):电池剩余电量、电池充电状态(是否在充电)、充电温度(温度太高时自动断开充电)、使能控制是否充电(可以IO控制)
  3. 输入5V、输出5V
  4. 电池供电时,负载大约是500uA(系统休眠)~1.5A(系统工作)
  5. 使用一颗或者多颗芯片完成上述功能