Other Parts Discussed in Thread: LMR14050, , LM431
我打算使用LMR14050绘制一个反向降压电路,输入电压为15V,输出电压、电流为-15V/0.2A,我注意到参考设计PMP10680中,LMR14050的EN引脚外接了一个由LM431组成的大电流稳压器,该电路作用如下图:
即输出电压Vo等于输入电压V+,既然如此,LMR14050的EN引脚为什么不直接与VIN引脚连接呢?附PMP10680参考设计:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
LMR14050的EN引脚为什么不直接与VIN引脚连接呢?
如果单纯为了应用您可以根据您的实际情况直接连接VIN,根据datasheet等均有这样的设计。
至于为什么不这样直接连在一起因为官方推荐参考设计有考虑到UVLO的阈值可以通过Ven的值来调节。
Enable pin, with internal pull-up current source. Pull below 1.2 V to disable. Float or connect to
VIN to enable. Adjust the input under voltage lockout with two resistors. See the Enable and
Adjusting Under voltage lockout section.
这是datasheet原文是通过接在EN管脚外部两个电阻来调节,实际就是调节Ven电压来改变UVLO阈值。这样在参考设计里方便客户根据自己的情况进行稳定的调节,当然,如果您只用两个电阻也可以,但是需要保证稳定供电,因为EN脚还涉及到使能。