This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25723: 接PC VBUS 5V可以充电,但接入PD充电头VBUS升压到15V后无法充电

Part Number: BQ25723

Hi TI,

我们产品使用的电池为两串最高电压8.8V的锂电池。
在接入PC或hub的时候,VBUS为5V,可以进行5V500mA的充电。
接入PD适配器后,当VBUS升压到15V后,电流为几百uA,可以认定为没有进行充电。
分别打印正常充电-异常充电的寄存器和PD充电前-PD充电后的寄存器,并没有发现什么异常:

我们抓了VBUS和CHRG_OK的波形:

蓝色:VBUS
黄色:CHRG_OK

后面我们有做过其他实验:当接入PD充电头后,让PDControler不要请求那么高电压,只请求9V,发现是可以正常充电的
但我们的产品设计上必须要支持15V基至20V供电。

请帮忙分析一下为什么升到15V后BQ25723无法充电?

thanks!