1、现设计一个5并10串的电池,放电时发现电量为14%左右时突然变为0,且静置一段时间后电量会从0上升一点点(大约340mAh),请问是何原因?此外之前做了一款4并10串的电池,5并与4并电芯一样,但是配置文件的CHEM-ID不同,是不是哪里有问题?
2、BQ34Z100可电量LED来粗略显示电量,我们外部用5颗LED。由于电池放电时需要预留部分电量,假设预留2000mAh(20%额定电量),我们认定剩余电量为2000mAh时的电量为0,显示器显示0%,但是电池上5颗LED仍有2颗点亮(20%-40%),两者不同步。请问BQ34Z100可否有参数设置,让剩余电量为2000mAh时LED点亮1颗(0%-20%)?